AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Help Needed: Undefined Reference Error in SPC5 Studio

Hi everyone, I've created a library and placed it in the directory /source/driver/. The library consists of the following files: source/driver/VN9d30Q100.hsource/driver/VN9d30Q100.c The problem I'm encountering is that when I try to use a function fr...

LuciferD_0-1718884762261.png
LuciferD by Associate II
  • 2610 Views
  • 1 replies
  • 0 kudos

Resolved! SPC560P50L3 MCU ID

Hello,The chip I am currently using is SPC560P50L3, I need a unique MCU ID for calculation, but I checked the MCU ID registers of the two chips and found that the information is the same, MIDR1=0x56042416, MIDR2=0xA8005011. is this normal?Or if there...

wybll_0-1717655092798.png wybll_1-1717655106165.png
wybll by Associate
  • 1134 Views
  • 1 replies
  • 0 kudos

Resolved! Hello! I want to ask a question about setting up EIRQ!

Hello! I would like to ask what is the meaning of setting the Latched state option in the red box as shown in the following figure? I didn't see any specific definition or explanation related to this in the SPC58 reference manual? Can you tell me whe...

QQ图片20240603110635.png
Bwang.3 by Associate III
  • 1725 Views
  • 1 replies
  • 0 kudos

Resolved! AutoDevKit Studio

Hello! I would like to ask what is the meaning of setting the Latched state option in the red box as shown in the following figure? I didn't see any specific definition or explanation related to this in the SPC58 reference manual? Can you tell me whe...

QQ图片20240603110635.png
Bwang.3 by Associate III
  • 1848 Views
  • 1 replies
  • 0 kudos

Resolved! Hello! Ask a question about the debugger!

May I use the onboard debugger on the SPC582B-DIS Discovery board to download debugging programs for the AEK-MOT-MR200G1 development board? Can you tell me which specific pins need to be connected? As shown in the following picture!

QQ图片20240527225204.png QQ图片20240527225444.png
Bwang.3 by Associate III
  • 2244 Views
  • 2 replies
  • 0 kudos

Resolved! OpenOCD common error .cfg path not found

Hi, If you are getting this kind of error when you try to run your OpenOCD in AutoDevKit Studio 2.2.1: Then most probably you have not updated the search path of the config files. From main AutoDevKit menu, select Run > Debug Configurations   In th...

MaxVIZZINI_0-1714465471083.png MaxVIZZINI_1-1714465545119.png MaxVIZZINI_2-1714465597562.png MaxVIZZINI_3-1714465679865.png