AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! AutoDevKit does not appears in zip folder.

Hi, I'm an SPC5 beginner. I followed the YouTube tutorial and correctly installed AutoDevKit zip file. When i go SPC5Studio>Help>Install New Software>Add>Local, AutoDevKit does not appears in my unziped folder. I see there are some files in the video...

Nurlan13 by Associate
  • 1741 Views
  • 1 replies
  • 1 kudos

Checking for availability of CanTp

Hi all,Good Afternoon, I hope all are doing goodIn my project I am implementing diagnostics, so now I need CanTp for sending and receiving the data which is more than 8bytes. Now I am using SendCanMessage() API for transmitting the data and mcanconf_...

Aishwaryaum_1-1722329849994.png

Resolved! Software Reset API

Hello all,A very good afternoon, I hope you all are doing goodI am implementing Diagnostics in my project and in the during the implementation of service 11 I am facing the issue for software rest, I want to know which API performs the software reset...

Aishwaryaum_0-1722328517926.png

Resolved! L9963E response frame error

Dear community member,I am using L9963E IC on custom pcb board. I send a command to read register address 0x02 of device 1, but in response frame getting address feedback for register address 0x06. also while reading dev_gen_cfg, getting different re...

bitBuddy_0-1721633596706.png bitBuddy_1-1721633873532.png bitBuddy_2-1721634364644.jpeg
bitBuddy by Associate II
  • 1668 Views
  • 1 replies
  • 0 kudos

Resolved! Issue with open load detection in PLAY mode.

Hi all,I am facing issue with Open Load detection in PLAY mode and it is working fine in MUTE mode.I have flashed and tested  the example base code from STM(Autodevkit), Open Load Detection is not working in PLAY mode in this code(Placed the example ...

Aishwaryaum_0-1719898606566.png Aishwaryaum_2-1719899332719.png Aishwaryaum_1-1719899285361.png Aishwaryaum_3-1719899723382.png

Resolved! Pin mode question for SPC582B using SPC5 Studio

Hello,I'm trying to start new project which is AVAS PRJ with SPC582B. So, I'm studying it with ST EVK like below.Anyway, When I check pin mode in AutoDevKitStudio, I don't understand exaclty the meaning of pin modes(MODE_IO/MODE_GPI/MODE_OUTPUT/MODE_...

decemberdream_0-1719366541509.png decemberdream_4-1719366846659.png