cancel
Showing results for 
Search instead for 
Did you mean: 

Autodevkit 2.2 CAN Examples missing, version bug

Orbiter
Senior

I uninstalled my prior Autodevkit 2.1 which seemed to had a lot of trouble with my workspace. 

The new 2.2 looked promising. A minor bug is that it still shows 2.1 in the About/help section as in the release notes, as on the linked website of the release notes. 

 

But most disturbing: I miss my examples from the application library! If I choose AEK-MCU-C2MLIT1 or SPC58EC I cant see any CAN example. Even if i filter for CAN I get some results of which some dont even contain any CAN. 

The RLA CAN Test Application for discovery is gone (I used it on 2.1), I can find it when I select SPC58x Gxx - which does not work (UDE can´t get contact and load this onto the board) 

I also can´t find a example update function or release note what the examples are doing in particular or which UM/release note may walk me through them. How is the usage intended? 

1 ACCEPTED SOLUTION

Accepted Solutions
Max VIZZINI
ST Employee

Attached you can find the CAN RLA example to be imported.

Unzip it and put it in a working folder or AutoDevKit workspace folder.

Go to File>Open projects from File System

2023-11-19 16_47_48-workspace - AutoDevKitStudio.png 

Generate and compile the code.

I have also attached a PDF document with basic explanation on CAN usage.

Regards,

AutoDevKit Team

View solution in original post

1 REPLY 1
Max VIZZINI
ST Employee

Attached you can find the CAN RLA example to be imported.

Unzip it and put it in a working folder or AutoDevKit workspace folder.

Go to File>Open projects from File System

2023-11-19 16_47_48-workspace - AutoDevKitStudio.png 

Generate and compile the code.

I have also attached a PDF document with basic explanation on CAN usage.

Regards,

AutoDevKit Team