Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Multiple VL53L0X sensors and I2C bus

I have an application that uses 10 VL53L0X sensors on an I2C bus.  I seem to have ended up damaging multiple STM32 dev boards trying to get this configuration to work reliably.  Any help to understand what I am doing wrong would be appreciated.So, th...

MikeB100 by Associate
  • 130 Views
  • 2 replies
  • 0 kudos

VL53L0X Arduino vs STM

Hello, I have multiple VL53L0X sensors that I am communicating with over an STM32 board. Two of the sensors started throwing errors (only reading 8191), and so I moved them to an Arduino for the flexibility of using the downloadable API. They worked ...

How to calibrate VL53L0x

Hi,     1》In the dark,Place the white target 140mm from the sensor          call function         Status = VL53L0X_perform_offset_calibration(&vl53l0x_dev,0x8c0000,&pOffsetMicroMeter);     2》In indoor environments ,Place the black target  600mm from ...

zhy by Associate III
  • 204 Views
  • 3 replies
  • 0 kudos