Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L1X: what is the difference between 2V8 and 1V8 mode

To use the VL53L1X with a 3V3 supply, I will have to select 2V8 mode.The default mode is 1V8 mode. The selection wil be done in 1V8 mode. Apperently I2C will function correct in 1V8 mode with a 3V3 supply.What is the difference between 1V8 and 2V8 mo...

PSimo by Associate
  • 2198 Views
  • 1 replies
  • 0 kudos

Can I power the VL53L1X with 3V3?

The typical IOVDD (2V8 mode) and AVDD of the VL53L1X may be 3V3 according the datasheet.In ST applications (for example the X-NUCLEO-53L1A1) a levelshifter is used to interface the 2V8 powered sensor with the 3V3 powered MCU.I want to use the VL53L1...

PSimo by Associate
  • 1025 Views
  • 1 replies
  • 1 kudos

VL53L0X Calibration

We are putting the VL53L0X in a device with a tinted lens cover. Example shown bellow. I wanted to know about the calibration process during manufacturing that is recommended in the Application note. Is the calibration different from each individua...

0690X00000ARAK2QAP.jpg
Tashfique by Associate II
  • 1890 Views
  • 1 replies
  • 0 kudos

i am trying to merge vl53l1x API to nrf52....it is giving me an errors to files "vl53l1_platform_user_data.h" "vl53l1_wait.h" the errors are unknown type name 'VL53L1_DevData_t'

request for member 'CurrentParameters' in something not a structure or unionrequest for member 'LLData' in something not a structure or unionrequest for member 'PalState' in something not a structure or union i am using nrf52832 and vl53l1x sensor

Apati.17 by Associate
  • 1341 Views
  • 3 replies
  • 0 kudos

broken TOF sensor vl53l0x

I am using the vl53l0x tof sensor in one of my products but I am currently experiencing a huge amount of fallout on this product.On a batch of 30, I had 10 broken VLX53l0x TOF sensors after soldering.What occured, the sensor started to pull down itse...

Jvan.10 by Associate II
  • 2404 Views
  • 4 replies
  • 1 kudos

Maybe an elegant way to address multiple VL53L1X sensors.

Can I use the GPIO1 from the first sensor on the I2C bus to control the XSHUT pin on the second sensor etc.Here is the plan.Assume that I do not use the GPIO1 pins to interrupt my microcontroller. I will use the API to check it there is new data. XS...

GAlbe by Associate II
  • 3217 Views
  • 6 replies
  • 0 kudos

Invalid range from VL6180X

I have the X-NUCLEO-6180XA1 board working with an STM32G071 Nucleo board. However the range reading doesn't seem to change when the range to the object changes. If there is nothing in range, I correctly read 0x72 from the range status register, but...

BCoch by Senior
  • 1350 Views
  • 2 replies
  • 0 kudos