Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L7CX current consumption

Dear ST,Now I'm testing my VL53L7CX sensor that is on the package P-NUCLEO-53L7A1 in Autonomous Mode with integration time = 2ms, ranging freq. = 4Hz and 4X4 Resolution, the attached screen-shot represents the output current related to my integration...

Resolved! Time-of-flight measuring level in a vertical pipe

Would it be possible to use a Time-of-flight sensor to measure water level in a pipe?The pipe is vertical with a diameter of 50 or 75 mm and a height  of 800 mm. At bottom there is a 90 degree bend. Sensor should be at top looking down the pipe. I as...

kurtm by Associate II
  • 315 Views
  • 5 replies
  • 3 kudos

Resolved! How to reduce power of VL53L0x

Hi, When performing two measurements per second, how can the power consumption of the VL53L0x be reduced? Is a single measurement or continuous timed measurements preferable? I adopted continuous timed high-speed measurements, setting the measurement...

zhy by Associate III
  • 233 Views
  • 1 replies
  • 0 kudos

Linux Driver Support for VD55H1 iToF Sensor (i.MX8MP)

Dear ST Support Team,I am writing to express my interest in the VD55H1 iToF sensor for an upcoming project.Currently, we are preparing for development using the i.MX8MP platform running on a Linux Kernel. Upon reviewing the technical specifications, ...

seobi by Associate
  • 315 Views
  • 2 replies
  • 0 kudos

VL53L8CX Driver software download

Hi - when I attempt to download the driver for this device the download never completes; I get a file "Unconfirmednnnn.crdownload" in my download folder. I'm using Edge browser on a Windows 11 Home 64 bit operating system. Using Norton, can't see any...

Resolved! VD6283 eval kit does not work with the GUI 1.0.1

Hi,I've P-NUCLEO-6283A1 and downloaded the graphical user interface STSW-IMG301. The quick start guide does not seem to be up to date as I did not find "VD6283_setup.exe" I was supposed to install, just a plain exe in the zip.At the first try GUI com...

Mulleteer_0-1776760979108.png Mulleteer_1-1776761230139.png

Resolved! VD55G4 Promodule

We will design a layout for the VD55G1 Promodule with Image read out over I3C. Alternative there is also a VD55G4 camera with an additional SPI image read out. Is it possible to get the pin assignment for the new VD55G4 promodule ?

Noeldi by Associate
  • 211 Views
  • 1 replies
  • 0 kudos