cancel
Showing results for 
Search instead for 
Did you mean: 

Is there anything provided by ST about Bluetooth LE audio?

승양.1
Associate

Hello

I'm going to use BLE to make a Bluetooth speaker that is connected to a cell phone.

As far as I know, I need to use I2S to use audio output, is there an MCU that supports BLE and I2S communication?

And can I know an example or something to refer to?

Thank you.

2 REPLIES 2
Imen.D
ST Employee

Hello @승양.1 and welcome to the STM32 Community =)

There is a large selection of STM32 microcontrollers which may answer your request.

I advise you to use the ST-MCU-FINDER tool (integrated also in STM32CubeMX) that allows an easy search of MCU with multiple criteria to ensure the selection of the right MCU. 

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Andrew Neil
Evangelist

Note that Audio over BLE is a pretty recent addition to the Bluetooth specs - are there many (any?) phone which support it yet?

" As far as I know, I need (sic) to use I2S to use audio output"

You don't need to - there are plenty of other ways to transport audio.

"can I know an example or something to refer to?"

putting "st ble audio" into google, the very first hit is:

0693W000007ZaxRQAS.png