cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STM32F746G-discovery kit with 6.1.1 CubeMX version and updated firmware. I have created a cubeMX default project and tried to build it. Build is successful but when I try to run that on the development kit, it does not download successfully.

Shruthi
Associate II

Info : STM32F746NGHx.cpu: hardware has 8 breakpoints, 4 watchpoints

Info : Listening on port 3333 for gdb connections

target halted due to debug-request, current mode: Thread 

xPSR: 0x01000000 pc: 0x0800b664 msp: 0x20050000

Info : Stlink adapter speed set to 1800 kHz

adapter speed: 1800 kHz

** Programming Started **

auto erase enabled

Info : flash size probed value 1024

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x20000084 msp: 0x20050000

wrote 65536 bytes from file Debug/PeripheralsTrial.elf in 1.273580s (50.252 KiB/s)

** Programming Finished **

** Verify Started **

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000002e msp: 0x20050000

verified 47680 bytes in 0.160581s (289.963 KiB/s)

** Verified OK **

** Resetting Target **

shutdown command invoked

I see that there are 8 breakpoints and 4 watchpoints in stmWorkbench. But I did not find which part of the project has this. I have also tried selecting option of 'remove all breakpoints in project' But still this error persists. Please help me with this. Im unable to start any project.

0 REPLIES 0