cancel
Showing results for 
Search instead for 
Did you mean: 

IOC file for LwIP_HTTP_Server_Netconn_RTOS Example project

MStra.3
Associate III

Is there an IOC file available for the LwIP_HTTP_Server_Netconn_RTOS Example project? I am working with the Nucleo-144 with the STM32F439ZI. Although the example project is for the 429, it works on this board. I want to be able to use CubeMX to add more middleware to the project.

Mike.

2 REPLIES 2
Houssem CHAABANI
Senior II

Dear @MStra.3​ ,

You can migrate the example from one STM32 to another by following this tutorial.

Hope that this solve your issue.

Best regards,

Houssem

MStra.3
Associate III

That is not what I asked for. I want an IOC file for the LwIP_HTTP_Server_Netconn_RTOS Example project so I can reconfigure the project using CubeMX.

Mike.