cancel
Showing results for 
Search instead for 
Did you mean: 

Getting errors accessing stm32cubeF0 in stm32cubeIDE (both v1.0.0 and v1.3.0)

peberg65
Associate

Tried to update to STM32CubeF0 V1.11.0 for the STM32CubeIDE v1.0.0 that I used.

From the Help -> Manage embedded software packages.

Getting an error about zip-file not available.

Installing a new instance of STM32CubeIDE v1.3.0.

Getting the same error for downloading when I try the Manage embedded software packages.0690X00000DXNOYQA5.png

OK, it says that I can load them manually with "From Local".

So I found the STM32CubeF0 v1.11.0 on ST.COM site and download it.

Hitting the "From Local" button and get this instead:

0690X00000DXNQAQA5.png

I try to unzip the file myself, no problem. No errors during the unrar unzipping of the file.

But I am not familiar enough with windows and installation process, so I don't know what to with the unzipped file anyway.

The problems arises inside of the STM32CubeIDE. So I don't think neither my network nor the zip-file is the problem.

Just as a test I tried to manage the following 2 packages with same result:

STM32CubeF0 V1.9.0

STM32CubeF4 V1.25.0

They both got similar error popup as the first image above.

Any advices on how to proceed to get this to work?

0 REPLIES 0