2020-02-26 8:06 AM
Tried to update to STM32CubeF0 V1.11.0 for the STM32CubeIDE v1.0.0 that I used.
From the Help -> Manage embedded software packages.
Getting an error about zip-file not available.
Installing a new instance of STM32CubeIDE v1.3.0.
Getting the same error for downloading when I try the Manage embedded software packages.
OK, it says that I can load them manually with "From Local".
So I found the STM32CubeF0 v1.11.0 on ST.COM site and download it.
Hitting the "From Local" button and get this instead:
I try to unzip the file myself, no problem. No errors during the unrar unzipping of the file.
But I am not familiar enough with windows and installation process, so I don't know what to with the unzipped file anyway.
The problems arises inside of the STM32CubeIDE. So I don't think neither my network nor the zip-file is the problem.
Just as a test I tried to manage the following 2 packages with same result:
STM32CubeF0 V1.9.0
STM32CubeF4 V1.25.0
They both got similar error popup as the first image above.
Any advices on how to proceed to get this to work?