cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 and accumulator

svarog995
Associate II
Posted on July 29, 2013 at 14:24

I have a question, I'm doing the robot. Is it possible to feed the controller from the battery and usb or is it dangerous?

1 REPLY 1
emalund
Associate III
Posted on July 29, 2013 at 15:04

 Is it possible to feed the controller from the battery and usb or is it dangerous?

 

 

should not be a problem using a couple of diodes

the dangerous part is if you try to charge the battery.

Erik