cancel
Showing results for 
Search instead for 
Did you mean: 

Command sequence for USART bootloader on stm32G4 MCU

shraddhs10
Associate II

Hello,

 

I am trying to flash the MCU with USART bootloader

I am using the command codes from below link, but are not working for me

Can someone help me validate of the command codes are correct for STM32G4

https://www.st.com/resource/en/application_note/cd00264342-usart-protocol-used-in-the-stm32-bootloader-stmicroelectronics.pdf

 

Current setup:

I have connected the STM32 USART4 to my R PI device. It gets enumerated as /dev/ttyUSB0

Below is the serial code using python

 

import serial
 
ser = serial.Serial(
        port='/dev/ttyUSB0',
        baudrate=57600,
        parity=serial.PARITY_EVEN,
        stopbits=serial.STOPBITS_ONE,
        bytesize=serial.EIGHTBITS,
        timeout=10
)
 
# Command to select the USART bootloader
ser.write(b'\x7F')
ser.read(1) # Reading 1 byte of data to check ACK from the MCU

TIA

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Nice catch @Tesla 

Even you didn't mention the exact G4 part number but UART4 is not used for G4 bootloader.

You can refer to the AN2606 tables Table 99 / Table 101 / Table 103: Only USART1, 2 and 3 are used for bootloader.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2

Going to be as described in AN2606 for the pins and AN3155 for the UART

Pretty sure UART4 has NO involvement, read and understand expectation from AN2606..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Nice catch @Tesla 

Even you didn't mention the exact G4 part number but UART4 is not used for G4 bootloader.

You can refer to the AN2606 tables Table 99 / Table 101 / Table 103: Only USART1, 2 and 3 are used for bootloader.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.