cancel
Showing results for 
Search instead for 
Did you mean: 

IAP code update

babidesai123
Associate II
Posted on November 19, 2003 at 12:04

IAP code update

1 REPLY 1
babidesai123
Associate II
Posted on May 17, 2011 at 11:56

Hi,

we are able to load the newapplication image on other flash using our own IAP routines.

Now we would like to try to program even the IAP code remotely using serial link.

Doubt:

1. Can we use CSBOOT0 as only block switching routine depending on whichever flash has valid sign byte programed.?

2. & IAP routines & actual boot code will be loded on CSBOOT1 or CSBOOT2 ( at one time any one will have valid IAP routines )

& primary flash FS1 & FS2 for application image ( at one time only one of the primary flash will have valid application image)

So that we can program any of the secondary or primary flash at run time!!

Even we would like to capture some of the critical information on CSBOOT3 ( will be in data space while writing information onto the same)

Purvi