2003-11-18 12:21 AM
flash programming to create in built log file
2011-05-17 02:56 AM
Hello,
We want to create a log file in the flash.so that without any console we can capture the data online. For that our IAP code resides in secondary flash & application code is in primary flash.Now we want to use the any one sector(8 KB) of secondary to capture the data send from primary flash. can we put the secondary flash(CSBOOT 2) in page 1 with some logic equation . & rest all secondary flash is at some other location with no page no. given to it. Purvi