cancel
Showing results for 
Search instead for 
Did you mean: 

STM32W108: SWO trace not working

gsegment
Associate
Posted on March 26, 2014 at 20:06

Hello,

I cannot start SWO trace (nothing received in debug window) with STM32 W108CB. I have standard configuration of ITM, listed below. And i configured the 33 pin for SWO with line ''REG_GPIOC->CRL = 0x900;''. Software used is uVision 4.76, jtag ULINK2.


static
int
Debug_ITMDebug = 0;




void
InitializeTrace(
void
)

{

volatile
uint *ITM_TER = (
volatile
uint *)0xE0000E00;

volatile
uint *SCB_DHCSR = (
volatile
uint *)0xE000EDF0;


*SCB_DHCSR = 0x30003;

*((
volatile
uint *)0xE000EDFC) = 0x01000000; 
// ''Debug Exception and Monitor Control Register (DEMCR)''

*((
volatile
uint *)0xE0042004) = 0x00000027;

*((
volatile
uint *)0xE00400F0) = 0x00000002; 
// ''Selected PIN Protocol Register'': Select which protocol to use for trace output (2: SWO)

*((
volatile
uint *)0xE0000FB0) = 0xC5ACCE55; 
// ITM Lock Access Register, C5ACCE55 enables more write access to Control Register 0xE00 :: 0xFFC

*((
volatile
uint *)0xE0000E80) = 0x00010009; 
// ITM Trace Control Register

*((
volatile
uint *)0xE0000E40) = 0x0000000F; 
// ITM Trace Privilege Register

*((
volatile
uint *)0xE0000E00) = 0x00000001; 
// ITM Trace Enable Register. Enabled tracing on stimulus ports. One bit per stimulus port.

*((
volatile
uint *)0xE0001000) = 0x400003FE; 
// DWT_CTRL

*((
volatile
uint *)0xE0040304) = 0x00000100; 
// Formatter and Flush Control Register


if
((*SCB_DHCSR & 1) && (*ITM_TER & 1)) 
// Enabled?

Debug_ITMDebug = 1;

}




void
TraceChar(
char
ch)

{

static
volatile
unsigned 
int
*ITM_STIM0 = (
volatile
unsigned 
int
*)0xE0000000; 
// ITM Port 0

static
volatile
unsigned 
int
*SCB_DEMCR = (
volatile
unsigned 
int
*)0xE000EDFC;


if
(Debug_ITMDebug && (*SCB_DEMCR & 0x01000000))

{

while
(*ITM_STIM0 == 0);


*((
volatile
char
*)ITM_STIM0) = ch;

}

}

2 REPLIES 2
Posted on March 26, 2014 at 20:25

Practically no support available here for the W108

The initialization seems like overkill, what's critical with SWO/SWV trace is that the CPU clock rate, and presumably ''baud'' rate,  is consistently understood. Keil expects the Core Clock to be correct.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nickname306_O
Senior
Posted on April 01, 2014 at 13:25

Hello kashlikov.sergey,

You are using JTAG as Debug Probe. Please switch to SWD (

Serial Wire Debug

).

The Serial Wire Trace Output pin (SWO) can be used in Serial Wire Debug mode only.

Best Regards,

Nouha