cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L072CZ Lora Keil License

Berni Bernd
Associate
Posted on May 04, 2018 at 13:54

Hi,

if I build the programm 'AT-Slave' (STMCubeExpansion_LRWAN) I got an License Error from Keil ( error: L6050U: The code size of this image (38072 bytes) exceeds the maximum allowed for this version of the linker.). It is possible to reduce the code size from the example without losing the function?

#at_slave #keil-mdk5 #b-l072z-lrwan1
1 REPLY 1
Posted on May 04, 2018 at 14:35

Use the free licence

http://www2.keil.com/stmicroelectronics-stm32/mdk

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..