User Activity

Hi everyone,I occasionally run into an error when flashing code to my board using the IDE. The error message is as follows: Failed to bind to port 61235, error code -1: No error Failure starting SWV server on TCP port: 61235 Failed to bind to por...
Title edited to reflect the correct board used. Changed from NUCLEO-H7A3ZI-Q to NUCLEO-H7S3L8.Hi,I’m trying to set up UART communication using UART3 on the NUCLEO-H7A3ZI-Q board. I have the UART3 pins (PD8 and PD9) connected to the ST-Link VCP on thi...
Hello ST Community,I have a question regarding the compatibility of the STLINK-V3MODS SWD pins with my MCU's SWD pins, which operate at 3.3V. Do I need to use logic level shifters between them, or are the STLINK-V3MODS SWD data signals fully compatib...
Hi everyone,I'm working with the STM32F429i-Disc1 board, writing code from scratch, and I encountered something odd. I created an empty project for the LCD, and during the LTDC pin initialization, I mistakenly set the alternate function (AF) to the w...
Hi St community,I noticed that the SB9 bridge on the STM32F429I-DISC1, which connects the SWO pin of the ST-Link to PB3 on the STM32, is ideally not soldered by default.Is there any specific reason for this? Does it affect the SWO functionality or de...
Kudos given to