cancel
Showing results for 
Search instead for 
Did you mean: 

Configure UART3 on NUCLEO-H7S3L8 Board for use with ST-Link VCP

Shreayas_Acharaya
Associate III

Title edited to reflect the correct board used. Changed from NUCLEO-H7A3ZI-Q to NUCLEO-H7S3L8.

Hi,
I’m trying to set up UART communication using UART3 on the NUCLEO-H7A3ZI-Q board. I have the UART3 pins (PD8 and PD9) connected to the ST-Link VCP on this board.

Do I need an external USB-UART converter to communicate through other UART pins, or should the onboard ST-Link handle the UART3 communication through VCP?
It's showing USART3 is not available.

Shreayas_Acharaya_0-1732541453113.png

 

I’m new to this board, so I want to confirm if there’s anything I might be missing in the configuration or connections. Any guidance would be appreciated!

Thanksin advance!

12 REPLIES 12

@Shreayas_Acharaya wrote:

Also, please clarify what this mean:


Is it this part that you're asking about:

AndrewNeil_2-1732704743344.png

Those are just the settings that you'd need for any UART link.

https://learn.sparkfun.com/tutorials/serial-communication/all

  • Baud rate (aka "speed") = 115200 bits per second (bps)
  • Number of data bits: 8
  • Parity: None (no parity bit)
  • Number of Stop bits: 1
  • Flow control: None (neither any "hardware" option nor any "software" option)
 

AndrewNeil_1-1732706774683.png

 

These are the settings that you always need to make whenever you connect any PC software to any COM port - virtual or otherwise.

For example, in TeraTerm:

AndrewNeil_1-1732704529760.png

In Device Manager:

AndrewNeil_3-1732704849896.png

Or at a "DOS Prompt":

AndrewNeil_4-1732705231085.png

 

So all exactly the same as you would for a real COM port, or any other USB-to-UART device (FTDI, in the above examples).

Your microcontroller code also needs to match these settings (hopefully, CubeMX does this for you).

 

mƎALLEm
ST Employee

Hello,

As a workaround, go to the Bsp menu and activate the Virtual Com port then deactivate it , then go back to USART3 under connectivity and you will be able to configure it. 

SofLit_0-1732705241412.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you, Neil, for clarifying.