Hello @devinw,Here are some steps that can help you resolve issues related to DFU firmware:Check BOOT0 and BOOT1 Pins: Ensure that the BOOT0 pin is set to high (1) and BOOT1 pin is set to low (0).Connect USB Cable: Connect the USB cable to the boar...
Hello @Lu Entong,This could be due to several reasons, such as incorrect handling of the I2C address or timing issues. Here are some steps that can help you:- Check that the system clock is correctly configured.- Configure I2C peripherals and GPIO pi...
Hello @dip , You can erase the memory of your STM32F407G-DISC1 using some tools provided by ST.Erasing Memory Using CubeProgrammerCubeProgrammer, a tool provided by STMicroelectronics, allows you to manage this task efficiently.Here is a step-by-step...
Hello @Antonin_m84 , According to the VL53L8CX_ULD_driver_2.0.0, you can download it from the following link: Download Link.We have a CubeIDE_F401RE_Example_SPI, which contains an example SPI with the VL53L8CX, as shown in the image below.For the con...