User Activity

I lifted regression test code from the netxduo stack to attempt a websocket client, but the best I can achieve is a 400 response from the server.  Has anyone successfully using websockets with STM32 + netxduo?The following code resides inside app_net...
After updating Cube to v1.5 for my STM32H5 project (Nucleo-H563ZI), the ethernet stopped working except during the initial run after a load of the firmware with the debugger.  After a reset, either POR or via the debugger, pings to the board fail.  W...
I'm trying to maintain a directory structure in my CubeIDE project that contains an import of a third party repository, however the directory is erased when I regenerate the drivers after saving changes to the .ioc file.  I'm using Azure RTOS which c...
Has anyone successfully used the BSD addon for netxduo inside CubeIDE?  I followed the instructions at the top of https://learn.microsoft.com/en-us/azure/rtos/netx/netx-bsd/chapter2 (the #define TX_THREAD_EXTENSION_3 int bsd_errno needed a trailing s...
Kudos from
Kudos given to