Skip to main content
robmilne
Associate II
Mar 21, 2024 5:59 PM UTC
Solved

H5 1.2.0 and Cube 1.5 break ethernet

After updating Cube to v1.5 for my STM32H5 project (Nucleo-H563ZI), the ethernet stopped working except during the initial run after a load of the firmware with the debugger.  After a reset, either POR or via the debugger, pings to the board fail.  When I checkout an earlier version of the code that uses a Cube v1.4 .ioc file, and bypass the migration to v1.5, the ethernet behaves normally.  Has anyone else experienced a similar issue?

    This topic has been closed for replies.
    STeaBest answer
    ST Employee
    Apr 18, 2024 3:53 PM UTC

    Hello @robmilne ,

    I confirm the issue, I reported the issue internally.

    Internal ticket number: 179408. (This is an internal tracking number and is not accessible or usable by customers).

    Thank you.

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    5 replies

    STeaBest answer
    ST Employee
    Apr 18, 2024 3:53 PM UTC

    Hello @robmilne ,

    I confirm the issue, I reported the issue internally.

    Internal ticket number: 179408. (This is an internal tracking number and is not accessible or usable by customers).

    Thank you.

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    robmilne
    robmilneAuthor
    Associate II
    Apr 18, 2024 5:55 PM UTC

    Hi STea,

    Another issue, that is not a show stopper, is that POR/BOR reset will not allow the LAN8742 to function properly.  At the top of my main routine, I inspect the state of the RCC_RSR register and immediately issue a sw reset if it equals the default 0x0c000000 value.  Pin or software resets permit the ethernet transceiver to run properly.  I had the same issue on one of our prototype boards that uses an ethernet connector with integrated magnetics.

    -rob

    ST Employee
    May 13, 2024 4:17 PM UTC

    Hello @robmilne ,

    can you please share with me the project that caused the Ethernet to Fail with IDE1.15.
    regarding the problem with POR/BOR thank you for pointing this out. but I don't seem to see this kind of behavior on Nucleo boards.

    BR 

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Graduate
    May 25, 2024 5:17 PM UTC

    Hello @robmilne!

    Please look at https://community.st.com/t5/stm32-mcus-embedded-software/netxduo-not-working-with-a-static-ip-addresss/td-p/673975. Seems to be similar to what you're facing.

     

    Please let me know if that solution works for you.

     

    BR,

    FabioFly

    robmilne
    robmilneAuthor
    Associate II
    May 27, 2024 1:12 PM UTC

    Hi FabioFly,

    If you use Vin as rgw power source (JP2 to to 'VIN 5V'), it does not work on POR/BOR.  It works with a reset source of RCC_RSR_PINRSTF or RCC_RSR_SFTRSTF (I haven't checked WDG resets).

    I can get it to work if I monitor the reset source at the start of main.  The following is what I need to do to get it working.

    /* USER CODE BEGIN PTD */
     typedef enum reset_e {
     RCC_RESET_POR_BOR = 0, /*!< POR or BOR reset occurred (default) */
     RCC_RESET_PIN, /*!< Reset from pin occurred */
     RCC_RESET_SOFTWARE, /*!< system reset generated by the CPU */
     RCC_RESET_WWDG, /*!< window watchdog reset occurred from WWDG */
     RCC_RESET_IWDG, /*!< independent watchdog reset occurred */
     RCC_ILLEGAL_STOP_ENTRY, /*!< Illegal low-power mode reset occurred */
     RCC_RESET_UNKNOWN
     } reset_t;
    /* USER CODE END PTD */
    
    /* USER CODE BEGIN 0 */
    reset_t getReset(void)
    {
     /* HAL_RCC_GetResetSource() resets interrupt flags in RCC_RSR register */
     uint32_t reset_src=HAL_RCC_GetResetSource();
    
     if ((RCC_RSR_PINRSTF) == reset_src) {
     return RCC_RESET_PIN;
     }
     if ((RCC_RSR_PINRSTF | RCC_RSR_BORRSTF) == reset_src) {
     return RCC_RESET_POR_BOR;
     }
     if ((RCC_RSR_PINRSTF | RCC_RSR_SFTRSTF) == reset_src) {
     return RCC_RESET_SOFTWARE;
     }
     if ((RCC_RSR_PINRSTF | RCC_RSR_WWDGRSTF) == reset_src) {
     return RCC_RESET_WWDG;
     }
     if ((RCC_RSR_PINRSTF | RCC_RSR_IWDGRSTF) == reset_src) {
     return RCC_RESET_IWDG;
     }
     if ((RCC_RSR_PINRSTF | RCC_RSR_LPWRRSTF) == reset_src) {
     return RCC_ILLEGAL_STOP_ENTRY;
     }
     return RCC_RESET_UNKNOWN;
    }
    /* USER CODE END 0 */
    
    int main(void)
    {
     /* USER CODE BEGIN 1 */
     reset_t reset = getReset();
    
     if (RCC_RESET_POR_BOR == reset)
     {
    		volatile int i;
    
    		for (i = 0; i < 0x400000; i++) {};
    		HAL_NVIC_SystemReset();
     }
     ...
    
     /* USER CODE END 1 */

    -rob