I have develop a program on STM32F746G-DISCO revision B02 with QSPI N25Q128A13EF840ENow the new boards revision C03 use the QSPI W25Q128JVEIQ.I have copied the file W25Q128JVEIQ_STM32F746G-DISCO.stldr from CubeIDE 1.16 to the STM32 ST-LINK Utility\S...
I am using a STM32F429BI module + 7" LCD RGB to display the amplifier settings and also a vu-meter.https://it.aliexpress.com/item/1005002482177244.htmlhttp://www.audiodesignguide.com/sw1/20240507_215200.mp4I would like to increase the speed of refres...
I am starting some test with this modulehttps://it.aliexpress.com/item/1005002482177244.htmlwith 7” lcdI have found only one example that run but with TouchgfxI have got the same ioc from this example to generate a new code and insert the functions t...
I have found an information about this problem so the action to solve is here:1) download the last driver in the en.stm32cubef7-v1-17-2.zip archive with inside the w25q128j.h file2) put this w25q128j directory inside \Drivers\BSP\Components3) save pr...
STM32F746G-DISO ver. B-04 with N25Q128A13EF840E14:09:22 : Data read successfully14:09:22 : Time elapsed during the read operation is: 00:00:00.00714:09:25 : Memory Programming ...14:09:25 : Opening and parsing file: FinalMono_ver5.hex14:09:25 : File...