2024-09-21 09:00 PM
Hi,
I tried installing ARM Cmsis 6 Pack with STM32CubeIDE 1.16.1. It is having errors. I'm attaching the screenshot below -
Though ARM Cmsis 5 is working fine.!
2024-09-22 08:05 AM
If you're not using the latest version of STM32CubeIDE or CMSIS packs, try to update it.
2024-09-23 03:08 AM
Cmsis pack is not required. It is integrated in CubeIDE.