User Activity

Is there any STM32 in TSSOP-20 package with OSC_OUT pin for use with a crystal oscillator?Mark Jordan 
As I understand, the TSSOP20 version needs an external oscillator instead of a 8MHz crystal connected directly to the MCU pins. Is that correct?I'm asking because I have seen a board on AliExpress using this same processor with a 8MHz crystal.
 I'm trying to set TIM2 in PWM mode, but I'm getting weird results. CH1 to CH4 are enabled but CH3 on PA2 shows no output no matter I do. The weird thing happens when I try to remap TIM2. There are three remap options, Remap2 is the one I'm intereste...
Kudos from