Hello @Andrei Chichak This is a CubeMX generation problem, CubeMX calls HAL_ADCEx_MultimodeConfigChannel in the ADC2 config while this function should only be called with the ADC master (ADC1).The blue box function must therefore be removed:
Hello @AGP For further information on the configuration of the GPDMA, please refer to the following article How to configure the GPDMA , which provides detailed instructions on the creation of a project using the GPDMA and the associated setup.
Hello @istepne It could be also a linking issue within STM32CubeIDE that's causing this behavior. Ensure that there are no linked resources between the two projects: Select Properties-> Resource -> Linked Resources(Check if there are any links to pr...
Hello @ŁJura.1 The link you shared with us is unreachable. Could you please share your code here by using the option "Insert/Edit code simple".Otherwise, Can you ensure that the filter configuration is correctly set up. Here is an example of how to c...