cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE TouchGFX 4.24.0 not available in STM32CubeIDE

AWack
Associate III

Hi,

 

I´ve just created a new project with TouchGFXDesigner 4.24.0.

When trying to compile the project in STM32CubeIDE the theres no valid CMSIS package for this version...

Any idea?

Best regards,

Achim

4 REPLIES 4
Peter Allnutt
Associate III

Sorry I can't help. Here as I have the same issue.

Hello ST where is the TouchGFX 4.24 package for CubeMX/CubeIDE?

Regards

 

tmehok
Associate II

I do not know if this will give the post more attention but I would like to know about this issue as well. Although I do not know for sure it may be part of my issue on what I posted today.

AMars.4
Associate III

Maybe this? 

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/x-cube-touchgfx-4-24-0-is-out/td-p/683800

 

Note : TouchGFX Designer 4.24.0 MUST be used with STM32CubeMX 6.11.0 or above (link to download STM32CubeMX).

Attention : If X-CUBE-TOUCHGFX 4.24.0 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-24-0.zip file to install the new pack inside STM32CubeMX.

 

 

Thank you @AMars.4 This has allowed me to get 4.24 into CubeMX. Sadly I'm busy with something else just now and can't try further, but on the face of it this is our solution