cancel
Showing results for 
Search instead for 
Did you mean: 

Project for Nucleo Board with X-NUCLEO-IKA01A1

AMars.4
Associate III

Hello,

In the annex video it is mentioned that the project archive is available for the Nucleo board project with X-NUCLEO-IKA01A1, however when I download the materials archive it appears to be missing.

Could you confirm this is the case, if so would it be possible to make this project available for download also?

Many thanks,

Anthony

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi Anthony,

The link is below, I've just uploaded the sw example you requested: LAB03_260522.zip , this is Anomaly Detection use case based on current sensor Z-NUCLEO-IKA01A1 and Nucleo-L073, detecting the anomalies of portable USB ventilator (the one used during NEAI WS, reference within the WS slides).

https://drive.google.com/drive/folders/1KY7U9Ef92gOSMCevfmXQiFQCkdfQ3rg8

Best regards,

Bartosz

View solution in original post

4 REPLIES 4
Bartosz BORYNA
ST Employee

Hello Anthony,

Do you mean NEAI Studio workshop repository on the googledrive ?

Best regards,

Bartosz

AMars.4
Associate III

Hi Bartosz,

This may be what I am looking for, could you share the link?

Thanks,

Anthony

Hi Anthony,

The link is below, I've just uploaded the sw example you requested: LAB03_260522.zip , this is Anomaly Detection use case based on current sensor Z-NUCLEO-IKA01A1 and Nucleo-L073, detecting the anomalies of portable USB ventilator (the one used during NEAI WS, reference within the WS slides).

https://drive.google.com/drive/folders/1KY7U9Ef92gOSMCevfmXQiFQCkdfQ3rg8

Best regards,

Bartosz

AMars.4
Associate III

Hi Bartosz,

That's great, thank you! I will study that.

Anthony