Hi,I have tried to load a Project (.ioc file) build with CubeIDE 1.15.0 in the newly released CubeIDE1.16.0 (with CubeMX 6.12.0).This give me an error on ADC1:1) I can't select Vbat as ADC source (as working on CubeMX 6.11.0)2) I get a warning about ...
Updating to CubeIDE 1.14.1 I have seen that I can choose some new STM32H7xx MCU's ( especialy the STM32H725, STM32H735 and STM32H730 ). They are very interresting for me ( 3. CAN interface and 2x OCTOSPI with hyperflash support ). Is there any roadma...
Hi,As You can see in AN2606 the STM32H74x_H75x can only use PH13, PH14 for FDCAN in Bootloader mode, so You are out of luck on the LQFP144 and LQFP176 package.Martin
Hi STTwo-23Attached a sample .io file made with MX 6.11.0If You open it with MX 6.12.0 without migration the ADC1 is OK (Vbat is present and there is no error).If You migrate the file with MX 6.12.0 Vbat is missing and there is a error.
Hi,As described very well by Alex from APMemory: https://community.st.com/t5/stm32-mcus-products/where-is-it-documented-that-stm32h7-can-only-read-memory-mapped/m-p/598460/highlight/true#M225010There are some limitations on using QSPI /OSPI RAM chips...