2025-02-24 2:30 AM
Ther seems to be a problem in the STM32CubeIDE versione 1.17.0 when debugging / programming the STM32H730 chip.
The Programmer returns:
ST-LINK SN : 002800045553500F20393256
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.28V
Error: Unable to get core ID
Error: ST-LINK error (DEV_TARGET_CMD_ERR)
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 002800045553500F20393256
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x483
Revision ID : Rev Z
Error: Database: There's no active configuration for this device. All the 4 configurations are disabled!
Error: Database: There's no active configuration for this device. All the 4 configurations are disabled!
Device name : STM32H72x/STM32H73x
Flash size : 63 KBytes (default)
Device type : MCU
Device CPU : Cortex-M7
BL Version : --
Memory Programming ...
File : ST-LINK_GDB_server_a23924.srec
Size : 122.63 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing external memory sector 0
File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
Encountered Error when opening C:\ST\STM32CubeIDE_1.17.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.0.202409170845\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
Solved! Go to Solution.
2025-02-24 2:42 AM
2025-02-24 2:42 AM
2025-02-24 4:52 AM
How is it possible that a bug so obvious is not detected before a new SW release?
2025-02-24 9:14 PM
Just soldered up a new board design today with this MCU and am experiencing the same thing. I understand it's a known issue, but is there a temporary fix / estimate when it will be fixed? I need to get this board running as soon as possible