@Pavel A.Thank you peter for your reply.The problem is, that there is no OS FutureDescriptor in the original DFU SE sample code. (I could add, but that does not change tousand devices at customers)Even if i assign manual a winusb driver, the dfuSE De...
Hello, I'm a developer and need a working version of the Sttub30 .sys. Deletion is no solutio be cause we need to use it.All references to a Sttub30-w11-x64 from 2015 with newer version that is compatible with core isolation.But everything was delete...
How do I burn DFU files at ALL, after Win11 blocking the old dfudemo drivers?Win11 is blocking the drivers, if you have kernel isolation on. I can not ask my customer to disable security for this.Also stm32cubeprogrammer is listing my device as unkno...