User Activity

Hello to all,in our project we are using an STM32U5A5, and we need to be able to drive the sdcards at 1.8V if they are capable of it.We are using CubeMX to generate the basic code for initialization having configured the SDMMC1 to handle the transcei...
Hello,I'm using a STM32U5A5VJTXQ MCU and I need to use the 2K BKPSRAM located @0x40036400.I can read and write without problem the BKPSRAM after power up, but a power cycle corrupt all the content. Strangely, the RTC content: time and registers, are ...
Hello to all,I have some problems running HS USB MSC device type on a STM32U5 using AZURE. After the program is running on my board, I see this new device on the Device Manager of my PC:"Azure RTO USBX storage dev USBdevice".But there are no hard dri...
Hello to all, I create a new project using STM32CubeMX for the b-u585i-iot02a board. Then I added to the project the software and the library for the gesture recognition STSW-IMG035, specific to M33 processor. Compiling, I have this error:Description...
Hello to all, I'm trying to debug my multi core application. I'm following the AN5286 indication but I'm in stall soon, at "Shareble ST-Link"!I'm using Keil ver 5.31 and the ST-LINK is with firmware ver V3J5M2. The problem appear with one project sel...
Kudos from