User Activity

This is a really annoying problem which has existed for multiple releases of STM32CubeIDE. It is still present in 1.17.0.Procedure:- compile a new project- start a debugging session - step a few times, and exit- make some code changes- hit the Run bu...
I am working with STM32U073 and the LCD initialization code generated by CubeMx 6.12.0 (from STM32CubeIDE 1.16.0) does not work with LSI selected as the clock source.HAL_LCD_Init() returns HAL_TIMEOUT due to LCD_WaitForSynchro() timing out.The issue ...
The USB code for STM32H523 and STM32H533 generated by CubeMx v 6.12.1 (from STM32CubeIDE 1.16.1) does not work. It is missing a call to HAL_PWREx_EnableVddUSB() inside HAL_PCD_MspInit() The example code in:STM32Cube_FW_H5_V1.3.0\Projects\NUCLEO-H533R...
I am using a 32 MHz crystal with STM32U595 and I noticed that selecting HSE/2 (16 MHz) as OTG HS Clock Mux source results in USB_CoreReset() getting stuck in the loop waiting for the reset to complete:  do { count++; if (count > HAL_USB_T...
I am working on a project using USB HS with:STM32U595VJTSTM32CubeIDE 1.14.0STM32Cube_FW_U5_V1.4.0Using the init code, as generated by CubeMX, I was getting HAL_TIMEOUT returned by USB_CoreReset():MX_USB_OTG_HS_PCD_Init() -> HAL_PCD_Init() -> USB_Core...