User Activity

Hello to everyone,I'm working on the STM32F746NG Discovery Board to realize a simple audio effect and i need to use the audio codec WM8994. It is interfaced with the SAI2 audio peripheral. I dont want to use the HAL libraries but to write directly th...
Posted on November 21, 2016 at 20:59Hello everyone!I'm working with ST SPBLE-RF using the C code driver provided for BlueNRG-MS. I ported it for an ST8L151G6 microcontroller; the SPI communication works, the device answers correctly (0x02 and the R/...