cancel
Showing results for 
Search instead for 
Did you mean: 

How to launch STM32Cubeprogrammer in ubuntu can you please tell me.

MVENN.1
Associate II

i am not able to flash the image in stm32mp157c-dk2

43 REPLIES 43
Olivier GALLIEN
ST Employee

Hi @MVENN.1​ ,

Only the last version 2.6 is supported on Ubuntu 20.04.

And since this version the JRE is bundle inside STM32CubeProgrammer and no longer need extra JRE package.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

The installation PATH of STM32CubeProgrammer is not the good one as expected.

You have to install in "$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-2.5.0/" and add the binary path to path environment variable "export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-2.5.0/bin:$PATH"​

Armand

MVENN.1
Associate II

Hi Olivier GALLIEN (ST Employee )

Thank you for reply.

I am just installer STM32Cubeprogrammer 2.5.0 version in Ubuntu 20.04

can you please give steps to install the 2.6 version.

Thanks

please once check it. actually i installed everything but i did small mistake i don't know.

0693W000005CP0UQAW.jpg Thanks

Hi @MVENN.1​ ,

Download STM32CubePrg-Lin package here : https://www.st.com/en/development-tools/stm32cubeprog.html

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi Olivier GALLIEN (ST Employee)

Thanks its working fine.

when I launch and connect the device it shows like

I installed USB port also.

MVENN.1
Associate II

Hi Olivier GALLIEN (ST Employee)

I can able to install and connecting is ok but when i connect the device it showing like this please once check it.

0693W000005CT41QAG.jpgThank

MVENN.1
Associate II

please check i getting this warning

MVENN.1
Associate II

0693W000005CTHAQA4.jpg

MVENN.1
Associate II

When i flash the image in between connection is loss