cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to use STM32_Programmer_CLI when in the Starter-Package

Carson
Associate II

Hello,

 

I am following the wiki article: https://wiki.st.com/stm32mpu/wiki/STM32MP25_Evaluation_boards_-_Starter_Package, in order to bring up the STM32MP257F-EV1 Development board and I am unable to run the STM32_Programmer_CLI when trying to boot the board. I am able to run it when in my home directory but that's it. The instructions in section 2.1 in the wiki article don't seem to work and I am unsure if I am doing it wrong. Here are the paths to the CLI and the Starter-Package respectively:

STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32_Programmer_CLI

 

/STM32MPU-Ecosystem-v5.1.0/Starter-Package/stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/images/stm32mp2

Any help would be greatly appreciated. Thanks!

0 REPLIES 0