Unable to flash with STM32CubeProgrammer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-29 10:08 AM
Hi,
I just installed STM32CubeProgrammer v2.17.0 on Linux.
When I connect to the board (tried with several different ones), I get the following error;
flash loader cannot be loaded. FlashLoaderPath = /home/[yadayada]/bin/FlashLoader/0x
I can read the flash, I can do everything, with the exception of flashing. This fails.
I first thought it might be a truncated log message. But when I just copied any of the loader files and gave it the file name "0x", I didn't get the error message. So it really looks for a file named "0x". It looks like in the code, the assembly of the file name (all the files match the pattern 0x*.stldr)
I tried to do an software update, but this also fails: "The updater package on server is corrupted"
- Labels:
-
Bug-report
-
STM32CubeProgrammer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-29 10:45 AM
Hi,
I have IDE and Cube Programmer on Linux since years, no such problem.
So maybe you do something wrong or the package was damaged ( but very rare ).
So show, what Cube Programmer showing...
Or try full chip erase - if something crazy is there. Check option bytes for protection on some flash areas, set on unprotected then.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-29 11:11 AM
Thanks for the respone! I tried full erase. Also fails, with an error stating I should check write protection flags. But when I try to unset them, I again get an error. I just installed the program and started it. With and without sudo, no change. But what I do not have yet is the IDE. Maybe this sets an environment variable which is used by the programmer... Will try later today. I mean - what could I do wrong which results in the tool trying to open a flashLoader file named "0x"? It definetly is an error of the assembly of the file name (filename = "0x" + something + ".stldr")
Of course it is probably something with my configuration as it works for you. Maybe the missing IDE, even though it shouldn't.
Or do I miss something? Do I have to explicitely configure the FlashFile somewhere?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-29 12:04 PM
If you dont have IDE - how you make the program ?
For flash you just need a bin or HEX file, for the cpu you have. No mods needed,.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-29 12:21 PM
I am about to install the IDE. I just started with the programmer to check if I can talk to an eval board. That's why I wonder. My tool chain is not even yet installed, and to my understanding the programmer should be standalone. So no real room for me to do things wrong. My best suggestion is some env var provided by the ide, so it works for all who have the IDE installed, which I would consider a bug (production site for example needs a programmer but no IDE. I will try later today
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-29 1:39 PM
Hm, very strange. I installed the IDE, and using it, I can debug my code on the device. Also, after power-cycling the device, I can connect to Cube Programmer, and I see my code. So the IDE can flash without a problem. Just the standalone programmer can't. You sure can also flash your devices with the programmer standalone tool, right? I tried uninstalling, reinstalling - no luck. But at least at the moment I don't really need it as I can flash using the IDE. But it's strange....
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-30 3:37 PM
I have no idea why, but upgrading to Ubuntu 24.04 (from 22.04) resolved the issue.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-20 11:50 AM
I have similar problem. These started after I updated STM32CubeProgrammer to v2.17.0.
All works fine if a have that correct flash loader renamed to "0x", MCU flashes and it boots and the code in it works.
Here's the log with that "0x" file present
21:34:16:721 : UR connection mode is defined with the HWrst reset mode
21:34:16:760 : ST-LINK SN : 13001200042D363637365744
21:34:16:760 : ST-LINK FW : V2J37S7
21:34:16:760 : Board : --
21:34:16:761 : Voltage : 3.23V
21:34:16:761 : SWD freq : 4000 KHz
21:34:16:761 : Connect mode: Under Reset
21:34:16:761 : Reset mode : Hardware reset
21:34:16:761 : Device ID : 0x431
21:34:16:761 : Revision ID : Rev A
21:34:16:762 : Database: Config 0 is active.
21:34:16:762 : flash loader /home/jyko/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/FlashLoader/0x is loaded <--- Had loader for my MCU (f411) named to "0x" without any extension
21:34:16:762 : Debug in Low Power mode is not supported for this device.
21:34:16:922 : UPLOADING OPTION BYTES DATA ...
21:34:16:922 : Bank : 0x00
21:34:16:922 : Address : 0x40023c14
21:34:16:922 : Size : 8 Bytes
21:34:16:922 : UPLOADING OPTION BYTES DATA ...
21:34:16:923 : Bank : 0x00
21:34:16:923 : Address : 0x40023c14
21:34:16:923 : Size : 8 Bytes
21:34:16:923 : UPLOADING ...
21:34:16:923 : Size : 1024 Bytes
21:34:16:923 : Address : 0x8000000
21:34:16:923 : Read progress:
21:34:16:923 : Data read successfully
21:34:16:923 : Time elapsed during the read operation is: 00:00:00.008
21:34:38:205 : Memory Programming ...
21:34:38:205 : Opening and parsing file: Blackpill_f411.elf
21:34:38:206 : File : Blackpill_f411.elf
21:34:38:206 : Size : 18.78 KB
21:34:38:206 : Address : 0x08000000
21:34:38:206 : Erasing memory corresponding to segment 0:
21:34:38:206 : Memory Erase via FlashLoader!
21:34:38:206 : Memory erase...
21:34:38:206 : halt ap 0
21:34:38:238 : Erasing internal memory sectors [0 1]
21:34:38:238 : Init flashloader...
21:34:38:238 : halt ap 0
21:34:38:241 : run ap 0
21:34:38:242 : halt ap 0
21:34:38:242 : Loader sector erase...
21:34:38:249 : run ap 0
21:34:38:628 : halt ap 0
21:34:38:629 : Download in Progress:
21:34:38:629 : Size : 19232 Bytes
21:34:38:629 : Address : 0x08000000
21:34:38:629 : halt ap 0
21:34:38:649 : Loader write range...
21:34:38:708 : Init flashloader...
21:34:38:709 : halt ap 0
21:34:38:716 : run ap 0
21:34:38:717 : halt ap 0
21:34:38:728 : run ap 0
21:34:38:809 : run ap 0
21:34:38:886 : Segment[0] downloaded successfully
21:34:38:887 : File download complete
21:34:38:900 : Time elapsed during download operation: 00:00:00.682
21:34:43:348 : Disconnected
21:34:43:348 : Disconnected from device.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-07 7:51 AM
How did you identify which of the loader files in STM32CubeProgrammer/bin/FlashLoader was the right one to rename? I'm trying to flash an stm32f3discovery (stm32f303vc) but I can't figure out which of the files to rename. I can find files that are named close such as
0x32.stldr
but I couldn't find a file name that suggests it is appropriate for the target.
It would be nice if ST would fix this bug. It looks like the search path name is truncated.
In the mean time, I will continue to use tools that actually work (st-flash, openocd, gdb-multiarch etc).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-10 12:59 AM
Hello @AMacd.1 ,
Try using CubeProgrammer v2.18, the issue might be resolved. If not please specify the exact steps to reproduce. Since on my side I have tried reproducing this issue many times but failed.
Aziz
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.