21:34:16:721 : UR connection mode is defined with the HWrst reset mode 21:34:16:760 : ST-LINK SN : 13001200042D363637365744 21:34:16:760 : ST-LINK FW : V2J37S7 21:34:16:760 : Board : -- 21:34:16:761 : Voltage : 3.23V 21:34:16:761 : SWD freq : 4000 KHz 21:34:16:761 : Connect mode: Under Reset 21:34:16:761 : Reset mode : Hardware reset 21:34:16:761 : Device ID : 0x431 21:34:16:761 : Revision ID : Rev A 21:34:16:762 : Database: Config 0 is active. 21:34:16:762 : flash loader /home/jyko/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/FlashLoader/0x is loaded <--- Had loader for my MCU (f411) named to "0x" without any extension 21:34:16:762 : Debug in Low Power mode is not supported for this device. 21:34:16:922 : UPLOADING OPTION BYTES DATA ... 21:34:16:922 : Bank : 0x00 21:34:16:922 : Address : 0x40023c14 21:34:16:922 : Size : 8 Bytes 21:34:16:922 : UPLOADING OPTION BYTES DATA ... 21:34:16:923 : Bank : 0x00 21:34:16:923 : Address : 0x40023c14 21:34:16:923 : Size : 8 Bytes 21:34:16:923 : UPLOADING ... 21:34:16:923 : Size : 1024 Bytes 21:34:16:923 : Address : 0x8000000 21:34:16:923 : Read progress: 21:34:16:923 : Data read successfully 21:34:16:923 : Time elapsed during the read operation is: 00:00:00.008 21:34:38:205 : Memory Programming ... 21:34:38:205 : Opening and parsing file: Blackpill_f411.elf 21:34:38:206 : File : Blackpill_f411.elf 21:34:38:206 : Size : 18.78 KB 21:34:38:206 : Address : 0x08000000 21:34:38:206 : Erasing memory corresponding to segment 0: 21:34:38:206 : Memory Erase via FlashLoader! 21:34:38:206 : Memory erase... 21:34:38:206 : halt ap 0 21:34:38:238 : Erasing internal memory sectors [0 1] 21:34:38:238 : Init flashloader... 21:34:38:238 : halt ap 0 21:34:38:241 : run ap 0 21:34:38:242 : halt ap 0 21:34:38:242 : Loader sector erase... 21:34:38:249 : run ap 0 21:34:38:628 : halt ap 0 21:34:38:629 : Download in Progress: 21:34:38:629 : Size : 19232 Bytes 21:34:38:629 : Address : 0x08000000 21:34:38:629 : halt ap 0 21:34:38:649 : Loader write range... 21:34:38:708 : Init flashloader... 21:34:38:709 : halt ap 0 21:34:38:716 : run ap 0 21:34:38:717 : halt ap 0 21:34:38:728 : run ap 0 21:34:38:809 : run ap 0 21:34:38:886 : Segment[0] downloaded successfully 21:34:38:887 : File download complete 21:34:38:900 : Time elapsed during download operation: 00:00:00.682 21:34:43:348 : Disconnected 21:34:43:348 : Disconnected from device.