2024-12-19 02:18 AM - last edited on 2024-12-19 02:43 AM by SofLit
Hi STM32 enthusiasts,
I’m reaching out to the community for advice and guidance on an issue we’re facing while developing an external loader for our custom board. We’ve been working with the STM32H730IBK6Q chip and an external memory MX25LM51245GXDI00, and the hardware setup closely resembles the architecture of the STM32H735G-DK board.
In fact, our software was initially developed and successfully tested on the STM32H735G-DK, and we’re confident in its functionality on that platform. However, moving to our custom board with the STM32H730, we’ve encountered persistent issues with generating a working external loader.
Development on Linux using CubeIDE:
Testing on RAM using CubeIDE showed that both the Init function and external memory mapping worked flawlessly. Additionally, the MassErase function also worked as expected.
Issue:
11:04:17:021 : w ap 0 reg 12 R12 0x00000000
11:04:17:021 : w ap 0 reg 13 SP 0x00000000
11:04:17:021 : w ap 0 reg 14 LR 0x00000000
11:04:17:021 : w ap 0 reg 15 PC 0x240020FD
11:04:17:022 : w ap 0 reg 16 xPSR 0x01000000
11:04:17:022 : w ap 0 reg 17 MSP 0x00000000
11:04:17:022 : w ap 0 reg 18 PSP 0x00000000
11:04:17:022 : run ap 0
11:04:17:022 : halt ap 0
11:04:17:022 : r ap 0 reg 0 R0 0x240049B8
11:04:17:022 : Init function fail
11:04:17:022 : r ap 0 reg 16 xPSR 0x61000003
11:04:17:023 : halt ap 0
11:04:17:023 : w ap 0 reg 15 PC (0x24000000)
11:04:17:023 : w ap 0 reg 17 MSP (0x24000500)
2 . Testing with IAR:
Using IAR, we generated an external loader for the STM32H735G-DK, and it worked flawlessly:
Since the only theoretical difference between our custom STM32H730 board and the STM32H735G-DK is three GPIO pins, we modified the IAR project for the STM32H735 to match the custom hardware setup. Specifically, we changed the following pin configurations:
/**OCTOSPI1 GPIO Configuration
PD7 ------> OCTOSPIM_P1_IO7
PD5 ------> OCTOSPIM_P1_IO5
PG6 ------> OCTOSPIM_P1_NCS
PD13 ------> OCTOSPIM_P1_IO3
PD11 ------> OCTOSPIM_P1_IO0
PD12 ------> OCTOSPIM_P1_IO1
PF10 ------> OCTOSPIM_P1_CLK
PC2 ------> OCTOSPIM_P1_IO2 // change
PC3 ------> OCTOSPIM_P1_IO6 // change
PH2 ------> OCTOSPIM_P1_IO4 // change
PB2 ------> OCTOSPIM_P1_DQS
Issue: Despite these changes, the external loader failed on the custom board.
Analyzing the Problem:
We’ve carefully reviewed dozens of posts and suggestions from this community (a big shoutout to @Tesla DeLorean for their excellent insights), but we’re still stuck. The primary challenge is to get the external loader to work seamlessly, especially for debugging the external flash.
We’re hoping the collective wisdom of this community can shed light on what we might be missing. Thank you so much for your time and help!
Best regards
Emo