SWD connection no longer working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-10 8:51 AM
Hello,
On a STM32L4 design, we no longer have an SWD connection to the processor: using STM32CubeProgrammer reports
ST-LINK SN : 39FF6A064243383912381057
ST-LINK FW : V2J36S7
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x461
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 20 Bytes
Bank : 0x01
Address : 0x40022044
Size : 16 Bytes
UPLOADING ...
Size : 1024 Bytes
Address : 0x8000000
Read progress:
Error: Data read failed
SWD works fine in the design in general, also also ran on this particular device. An idea what is missing?
Or to put it the other way round: what do we need for a running SWD? Supply, connection to the SWD pins of course, but what further? IMHO we don't need running CPU core or clocking on it for example....
Thank you
Ralph
Solved! Go to Solution.
- Labels:
-
STM32CubeProgrammer
-
STM32L4 series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-22 7:07 AM
Hi @RHaag.1​ ,
Writing OB needs a specific procedure describes in MCU reference manual : "FLASH option bytes" section.
It is different from writing to flash.
The two OB BFB2 and RDP are configured in the same register , may be your are modifying the RDP when BFB2 is modified by your application.
Hope this helps you, when your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-14 12:54 PM
Hi @RHaag.1​ ,
I see in your log file that you are connecting in normal mode, can you please try to connect in "under reset" mode?
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-14 1:29 PM
Is hardware reset pin connected?
Select connect under reset.
Otherwise pull BOOT0 high and check if you recover connectivity.
Then check if you power down the hardware in your code, or interfere with the PA13/PA14 pins.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-15 10:51 AM
Thank you for your suggestions guys.
Connecting under reset didn' change the behaviour.
BOOT0 is no accessible in the desgin.
Meanwhile I learned I misinterpreted the tool output: I was indeed successfully connected via SWD, but the tools "auto flash read" function caused the error message! For whatever reason, the RDP byte in the option bytes was set to 0xFF which means level 1 and no access to user flash via SWD...strange thing
Regards
Ralph
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-20 2:37 PM
Hi @RHaag.1​ ,
If I well understand , when you set RDP to level 0 you are able to connect successfully?
Concerning the 0xFF value , your application is modifying any option bytes?
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-22 12:07 AM
Hi Houda,
I'm always connected via SWD (see my update below...) and yes, user flash can be read again after setting RDP to level 0.
My app can write a small part of OBs user byte: the bit BFB2 to switch between flash banks.
By the way: how are options bytes written in detail? Is it a "read erase write" like normal flash?
Regards
Ralph
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-22 7:07 AM
Hi @RHaag.1​ ,
Writing OB needs a specific procedure describes in MCU reference manual : "FLASH option bytes" section.
It is different from writing to flash.
The two OB BFB2 and RDP are configured in the same register , may be your are modifying the RDP when BFB2 is modified by your application.
Hope this helps you, when your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-23 2:26 AM
Hi Houda,
I know about the writing of option bytes and this is a very rare case in our application. But thanks for pointing out that both BfB2 and RDP are located in the same register, had not really realized that!
Also read the option bytes chapter in the manual again! Unfortunatelly, I didn't check the OPTVERR bit before overwritting RDP, but how about RDPs default level in case of "inversion data mismatch" in OBs: level 1 is used as default level, but what is the acutal register content in that case? Could it be the 0xFF I was reading?
Regards
Ralph
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-23 7:19 AM
Hi @RHaag.1​ ,
For RDP default value is 0xAA (as you can see in the snapshot I sent you the ST production value is 0FFEF F8AA).
Can you please tell me what do you mean by the "inversion data mismatch" in OBs? it is not a known notion for me.
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-23 11:26 PM
Hi Houda,
RM0351 3.4.2 Option bytes programming says:
If the comparison between the word and its complement fails, a status bit OPTVERR is set.
Mismatch values are forced into the option registers:
...
For RDP option, the value of mismatch is the default value “Level 1�?
The 0xAA you mention is the RDP reset value leading to "level 0", but which value in is forced to the RDP regs in the described mismatch case leading to "level 1"? Can't find it in the ref manual.
Regards
Ralph