cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4Q5CGT - not detecting in STM cube programmer

PJose.3
Associate II

Hi All,

We had purchased STM32L4Q5CGT6 controller for our work and after assembling and testing programming using STLINK V3 using SWD we found that none of the controllers are being detected in the programmer software. when connected the following screen appears

"Failed to connect to STM32 target".

we tested for 10 numbers of controllers and found the same issue in each. Is it due to the RDP feature or controller fail. If it is RDP then how can we remove the read out protection and program them. Any detailed step by step procedure is available, please suggest.

Thanks in advance.

Note - tried to add the images in screenshot but not able to add due to some error messages.

1 ACCEPTED SOLUTION

Accepted Solutions

STM32L4Q5CGT6 Expected/Wanted

STM32L4Q5CGT6P Purchased (Less Popular, More Available)

0693W00000SueCVQAZ.jpg 

https://www.st.com/resource/en/datasheet/stm32l4q5ag.pdf

I personally would have chosen a different Marking/SKU strategy, but..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

9 REPLIES 9
Amel NASRI
ST Employee

Hi @Community member​ ,

Most probably you need to perform an ST-Link Firmware Upgrade.

For more hints, please refer to How to solve debugger connection issues?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

PJose.3
Associate II

Hi Amel

thanks for your reply

When connecting the controller then the ST Link V3 is not able to detect the controller. I updated the firmware using another controller and STM V3Link. When I connect the STM32L4Q5CGT controller there is a fail message that appears. That's why I am not able to use stm cube programmer or cube ide for programming or full erase none of the options are working.

Thanks

0693W00000SubCwQAJ.png

The failure message says what?

If it can't find the STM32L4 it is likely not connected ​or powered properly.

Check orientation of part.

Check VDDA/VSSA.

Check level of NRST pin.

P​rovide relevant subset of schematic built, and wiring to the pod.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi

The relevant part is shown in the image. we have the same copy with different l4q5 controller working perfectly. The problem is only with this latest set of 10 numbers that we purchased recently.

Schematic wise all connections are right and tested

Thanks for your support

0693W00000SubzeQAB.png

So perhaps counterfeit?

Attach a large, clear and in-focus picture of part.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

0693W00000SucFDQAZ.jpg0693W00000SucF8QAJ.jpg 

the 2 images attached one is close up(assembled piece) and other one is IC packed one

That's a P suffix device, isn't that wired/powered differently?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

STM32L4Q5CGT6 Expected/Wanted

STM32L4Q5CGT6P Purchased (Less Popular, More Available)

0693W00000SueCVQAZ.jpg 

https://www.st.com/resource/en/datasheet/stm32l4q5ag.pdf

I personally would have chosen a different Marking/SKU strategy, but..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi

Ohh sorry I need to check that again. Thanks. Actually the issue was we could not get the same item elsewhere in any of the stores.

Thanks