cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer STM32G474 option bytes

FWege.1
Associate III

Dear all

I think the description is wrong or BOOT0/BOOT1 is swapped - see attachments.

If the option bytes are programmed as shown under STM32CubeProgrammer.png, the controller boots from flash.

Thanks in advance,

Franz

1 REPLY 1
KiptonM
Lead

Yes they are. I found out the hard way when it did not work. It was pointed out to me to use the documentation (Reference Manual) and that works.