cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CUBEprogrammer software bug

zhaowhong
Associate III
This software has too many bugs. Could the developers please look into the main issues? 1. If the downloader fails to connect, it spams dozens of error messages. 2. Frequent freezing, primarily when the downloader fails to connect—the software gets stuck and can't even be closed, which severely impacts usability.
 
5 REPLIES 5
mbarg.1
Lead

As most of us do not have such problems, please state your OS, sw version, CPU, ram ...

Imen.D
ST Employee

Hello @zhaowhong ,

Please share more data as mentioned by @mbarg.1 also the log file, to help you in your issues.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
TDK
Super User

No problems here.

If you feel a post has answered your question, please click "Accept as Solution".

When the software is in a connected state, there's an 80% chance it will freeze if the connected device loses power or the downloader becomes loose.

MGogr.1
Senior

No issues found on my device.