‎2018-08-08 02:42 AM
When starting install as described in documents, the setup icon appears and disappears directly. I tried to open the installer from the command line and then the following error message appears "LSOpenURLsWithRole() failed with error -10810 for the file /Users/joszelf/Downloads/en/SetupSTM32CubeProgrammer-1.1.0.app. "
Latest version of Java is installed. MacOS Latest version
‎2018-08-08 06:13 AM
these applications need java 8 and wont work with java 10.
also, st does not digitally sign their binaries, so the mac os puts it in quarantine
use the command
xattr -d com.apple.quarantine <the path to your installer>
to remove the quarantine flag
also, dont install as root into /Applications. install it as a normal user into somewhere else, such as Developer. same with the CubeMX application.
‎2018-09-25 08:44 AM
Hello @JVers.6​
Could you please specify the MAC Os version used?
This issue is raised internally for check and we will come back to you as soon as possible.
Kind Regards,
Imen.
‎2018-11-13 11:14 AM
Rather than launch the STM32Cube installer app, I selected the app, then Ctrl-Clicked to select "Show Package Contents". Next, Navigate to Contents>>macOs then Ctrl-Click on SetupSTM32CubeProgrammer-1_2_1_macos and select "Open" and the installer will run
‎2018-12-20 08:06 PM
Same issue with running the SetupSTM32CubeProgrammer-1.3.0
The command line running raises error:
➜ SetupSTM32CubeProgrammer-1.3.0.app /Applications/SetupSTM32CubeProgrammer-1.3.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-1_3_0_macos
Error: Unable to access jarfile ../../../SetupSTM32CubeProgrammer-1.3.0.exe
macOS 10.14.2
java -version
java version "1.8.0_121"
Java(TM) SE Runtime Environment (build 1.8.0_121-b13)
Java HotSpot(TM) 64-Bit Server VM (build 25.121-b13, mixed mode)
My previous installed STM32CubeMX app works normally.
‎2020-07-07 12:13 PM
Yeah, finally find the correct way to install. Helps me a lot! Thank you!😀
‎2020-07-12 05:44 PM
hello, did you solve your problem? i have the same issue
‎2020-07-12 06:52 PM
My recollection is that I dragged the existing app and associated folders to the trash, then installed.
‎2020-07-13 12:37 PM
After that the problem still exist, "..failed with error -1081" with the latsest Java edition
‎2023-09-02 06:04 AM
this way is work for me.