STM32CubeProgrammer: Error: Flash loader cannot be loaded
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-11 5:59 PM
Recently, I bought a clone of ST-Link V2.
I am trying to program a RAK5205 board with an STM32L151CB MCU on it, with a basic program for blinking LEDs.
If I use the STM32 ST-Link Utility v 4.5.0.0, open the file RAK5205_Blink.hex and program the MCU, it ends correctly and the program runs without problems on the board. If I want to completely erase the Flash memory, it does it correctly with this indication:
Device ID: 0x429
Device flash Size: 128KBytes
Device family: STM32L100x8xxA / L15xx8xxA
Flash memory erased.
Now, if I open the STM32CubeProgrammer v2.1.0, open the same file RAK5205_Blink.hex, the ST-Link v2 is recognized and connected correctly, read the memory of the MCU without problems, but when I want to program it in the same way than before, it shows the error, "Flash loader can not be loaded".
What is the difference between the ST-Link Utility and the STM32CubeProgrammer regarding device detection and programming?
What exactly does the error"Flash loader can not be loaded" means?
One difference I noted is that the STM32CubeProgramer, detected the Device as STM32L100x6xxA / STM32L100x8x ... with a Flash Size of 27520 KB instead of 128KB that has the MCU, different from what it is detected with ST-Link Utility.
Sorry if it is an stupid question, I'm a newby trying to lern. I'll appreciate any opinion or suggestion.
My OS is Windows 7 Ultimate.
Thank you
- Labels:
-
STM32CubeProgrammer
-
STM32L1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-18 12:33 AM
… I got the same issue with RAK811
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-01-18 8:19 AM
You must disable the read protection. The easiest way to do this is with the ST tool "Flash Loader Demonstrator". After a few next clicks you will find the option "Disable Read Protection" there. After that, you can check the "Option Bytes" with the STM32 ST-Link Utility. After that debugging ist running like a charm.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-28 9:18 AM
We have got the same issue:
- We use the STM32L151CBT6-A on a custom PCB. The hardware is properly installed. All supply pins are connected with their respective signals. The programming connections are fine.
- The software STM32CubeProgrammer is capable of reading the Flash and Option Bytes, but programming or erasing the flash results in the error message: "Error: Flash loader cannot be loaded". The same error occurs using the internal Debugger / Programmer in STM32CubeIDE.
- In contrast, flash programming is possible using the STM32 ST-LINK Utility by loading the .bin file. The programm is executed correctly.
I have no idea, what the source of this error might be. Since flashing and executing the program are both working fine after using the older ST-LINK Utility, the issue should be located inside the Toolchain / STM32CubeProgrammer.
Please respond to this entry if you are facing the same problem or have any ideas to solve the issue.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-02 8:26 AM
If anybody else is experiencing the same issue as mentioned in my previous post:
For me it works not to use the STM32 Cube Programmer (GUI / CLI or integrated in Cube IDE).
I have switched to openocd (Windows x64 binaries), either by opening a Debugging server manually or integrating the server start in Cube IDE. This works perfectly fine. My platform:
Windows 10 64 bit
Cube MX / IDE / Programmer
STLINKV2/1
The problem occured with STM32L151CB-A and STM32L152CB-A.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-22 4:04 AM
Same problem, it is not working to write with the STM32 Cube Programmer.
Target:
It does work with ST Visual Programmer and STM32 ST-Link Utility.
Windows 8 64 bit
Original ST-LINK/V2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-21 2:45 AM
I have also the same problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-21 4:00 AM
All the people on the thread have STM32L1 parts, running Windows, so I suspect you actually have a different problem
https://community.st.com/s/question/0D53W00000VivMBSAZ/access-the-flash-memory-from-stm32f767bi
The interaction with the device looks to be broken, so I'd assume some low-level drivers on the ST-LINK side.
Did the new version or the patch offered work?
Is the failure only in Ubuntu? Or did it follow you to Windows too?
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-21 6:51 AM
Hi,
In the Terminal "LSUSB" I find "ID xxxx:xxxx STMicroelectronics ST-LINK/V2". Some pages from the STM32F767BI are readable. I already install the latest linux driver for the ST-LINK/V2 version 1.0.3-1 from the packet en.stsw-linl007_V2-38-27.zip (other versions are windows only).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-25 7:05 AM
Still no sollution. They mention on google about st-link utility but this is integrated in the STM32 IDE.
Can someone help me out, if I run the IDE it gives the result below:
STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.6.0-RC3
-------------------------------------------------------------------
ST-LINK SN : 55FF6D066684564928211687
ST-LINK FW : V2J37S7
Board : --
Voltage : 3,26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x451
Revision ID : Rev Z
Device name : STM32F76x/STM32F77x
Flash size : 63 KBytes (default)
Device type : MCU
Device CPU : Cortex-M7
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_lSOXfX.srec
File : ST-LINK_GDB_server_lSOXfX.srec
Size : 6092 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing external memory sector 0
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening /opt/st/stm32cubeide_1.5.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_1.5.0.202011040924/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...