2019-06-11 5:59 PM
Recently, I bought a clone of ST-Link V2.
I am trying to program a RAK5205 board with an STM32L151CB MCU on it, with a basic program for blinking LEDs.
If I use the STM32 ST-Link Utility v 4.5.0.0, open the file RAK5205_Blink.hex and program the MCU, it ends correctly and the program runs without problems on the board. If I want to completely erase the Flash memory, it does it correctly with this indication:
Device ID: 0x429
Device flash Size: 128KBytes
Device family: STM32L100x8xxA / L15xx8xxA
Flash memory erased.
Now, if I open the STM32CubeProgrammer v2.1.0, open the same file RAK5205_Blink.hex, the ST-Link v2 is recognized and connected correctly, read the memory of the MCU without problems, but when I want to program it in the same way than before, it shows the error, "Flash loader can not be loaded".
What is the difference between the ST-Link Utility and the STM32CubeProgrammer regarding device detection and programming?
What exactly does the error"Flash loader can not be loaded" means?
One difference I noted is that the STM32CubeProgramer, detected the Device as STM32L100x6xxA / STM32L100x8x ... with a Flash Size of 27520 KB instead of 128KB that has the MCU, different from what it is detected with ST-Link Utility.
Sorry if it is an stupid question, I'm a newby trying to lern. I'll appreciate any opinion or suggestion.
My OS is Windows 7 Ultimate.
Thank you
2019-07-18 12:33 AM
… I got the same issue with RAK811
2020-01-18 8:19 AM
You must disable the read protection. The easiest way to do this is with the ST tool "Flash Loader Demonstrator". After a few next clicks you will find the option "Disable Read Protection" there. After that, you can check the "Option Bytes" with the STM32 ST-Link Utility. After that debugging ist running like a charm.
2020-09-28 9:18 AM
We have got the same issue:
I have no idea, what the source of this error might be. Since flashing and executing the program are both working fine after using the older ST-LINK Utility, the issue should be located inside the Toolchain / STM32CubeProgrammer.
Please respond to this entry if you are facing the same problem or have any ideas to solve the issue.
2020-10-02 8:26 AM
If anybody else is experiencing the same issue as mentioned in my previous post:
For me it works not to use the STM32 Cube Programmer (GUI / CLI or integrated in Cube IDE).
I have switched to openocd (Windows x64 binaries), either by opening a Debugging server manually or integrating the server start in Cube IDE. This works perfectly fine. My platform:
Windows 10 64 bit
Cube MX / IDE / Programmer
STLINKV2/1
The problem occured with STM32L151CB-A and STM32L152CB-A.
2020-10-22 4:04 AM
Same problem, it is not working to write with the STM32 Cube Programmer.
Target:
It does work with ST Visual Programmer and STM32 ST-Link Utility.
Windows 8 64 bit
Original ST-LINK/V2
2021-05-21 2:45 AM
I have also the same problem
2021-05-21 4:00 AM
All the people on the thread have STM32L1 parts, running Windows, so I suspect you actually have a different problem
https://community.st.com/s/question/0D53W00000VivMBSAZ/access-the-flash-memory-from-stm32f767bi
The interaction with the device looks to be broken, so I'd assume some low-level drivers on the ST-LINK side.
Did the new version or the patch offered work?
Is the failure only in Ubuntu? Or did it follow you to Windows too?
2021-05-21 6:51 AM
Hi,
In the Terminal "LSUSB" I find "ID xxxx:xxxx STMicroelectronics ST-LINK/V2". Some pages from the STM32F767BI are readable. I already install the latest linux driver for the ST-LINK/V2 version 1.0.3-1 from the packet en.stsw-linl007_V2-38-27.zip (other versions are windows only).
2021-05-25 7:05 AM
Still no sollution. They mention on google about st-link utility but this is integrated in the STM32 IDE.
Can someone help me out, if I run the IDE it gives the result below:
STMicroelectronics ST-LINK GDB server. Version 5.7.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.6.0-RC3
-------------------------------------------------------------------
ST-LINK SN : 55FF6D066684564928211687
ST-LINK FW : V2J37S7
Board : --
Voltage : 3,26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x451
Revision ID : Rev Z
Device name : STM32F76x/STM32F77x
Flash size : 63 KBytes (default)
Device type : MCU
Device CPU : Cortex-M7
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_lSOXfX.srec
File : ST-LINK_GDB_server_lSOXfX.srec
Size : 6092 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing external memory sector 0
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening /opt/st/stm32cubeide_1.5.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_1.5.0.202011040924/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...