cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer crashes when connecting to board.

CCend.2
Associate III

Hello,

I am following a tutorial to use AWS on my B-L475E-IOT01A board. When trying to program the board using STM32CubeProgrammer, it crashes when I click "connect" in the upper right hand corner. Sometimes it allows me to connect, but then crashes when I click on the "Erasing & programming" tab.

The program worked just fine the first time I used it to program the board, but this issue started happening after programming the board only a few times.

I am using STM32CubeProgrammer v2.13.0 on Ubuntu 22.04.2 LTS. The error log is pasted below:

#

# A fatal error has been detected by the Java Runtime Environment:

#

# SIGSEGV (0xb) at pc=0x00007f32916f5f2a, pid=2899, tid=0x00007f3281fc1640

#

# JRE version: OpenJDK Runtime Environment (8.0_265-b01) (build 1.8.0_265-b01)

# Java VM: OpenJDK 64-Bit Server VM (25.265-b01 mixed mode linux-amd64 compressed oops)

# Problematic frame:

# C [libstdc++.so.6+0xf5f2a] std::basic_string<char, std::char_traits<char>, std::allocator<char> >::basic_string(std::string const&)+0x1a

#

# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again

#

# If you would like to submit a bug report, please visit:

#  <snip>

# The crash happened outside the Java Virtual Machine in native code.

# See problematic frame for where to report the bug.

#

--------------- T H R E A D ---------------

Current thread (0x00007f32b058d800): JavaThread "JavaFX Application Thread" [_thread_in_native, id=2929, stack(0x00007f3281ec2000,0x00007f3281fc2000)]

siginfo: si_signo: 11 (SIGSEGV), si_code: 128 (SI_KERNEL), si_addr: 0x0000000000000000

0 REPLIES 0