2022-05-10 5:05 AM
Hello,
I cannot use the STM32CUBEprogrammer standalone program, however my programmer works just fine with stm32CUBEIDE V1.7. During programming in STM32cubeide the configuration is visible and it loads STM32cubeprogrammer V2.8 I copied the settings over to the standalone program since those seem to work in STM32CUBEIDE but it still does not work. I updated to the latest firmware and tried out both V2.9 and V2.8 of STM32CUBEprogrammer but neither works.
My settings: (from cubeide same settings used in cubeprogrammer)
ST-LINK SN : 6
ST-LINK FW : V2J39S7
Board : --
Voltage : 3.33V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x447
Revision ID : Rev Z
Device name : STM32L07x/L08x/L010
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0x__
I am using an ST-link compatible probe not an official one at the moment. The official one however does work. I dont mind using an official programmer but this one is a bit more convenient since it also can supply power.
https://opencircuit.nl/product/st-link-v2-stm8-stm32-programmer
Does anyone know why this problem happens? I dont think there is anything wrong with my connection. But it might be an incompatability between the official and this particular programmer, specifically with the standalone program but not the command line variant used in cubeide.
Solved! Go to Solution.
2022-05-10 5:52 AM
I tried ST-link and this works but instead of hardware and connect under reset. I needed to use software system reset and normal mode. For now my problem is solved since ST-link also has the features I needed (memory read) but I still find it weird that cubeprogrammer still fails to work. Whereas both ST-link and cubeIDE do work.
2022-05-10 5:52 AM
I tried ST-link and this works but instead of hardware and connect under reset. I needed to use software system reset and normal mode. For now my problem is solved since ST-link also has the features I needed (memory read) but I still find it weird that cubeprogrammer still fails to work. Whereas both ST-link and cubeIDE do work.
2022-05-12 12:30 AM
Hi,
You are free to use any debugger of your choice.
But, we as ST, cannot invest time in providing technical support for debug probes that we did not design nor manufacture..
Kind regards, Mattias
2022-05-12 4:17 AM
Hi,
That is ok, I thought maybe someone else encountered the same issue as me in the past and perhaps knows a solution.