2024-05-11 12:38 AM
Version: v2.16.0
I`ve downloaded and installed the latest application and was told that the CubeProgrammer could support J-Link now.
the GUI shows that JLink device can be selected:
I clicked the connect bottom, the chip select window of JLink was popped out:
after correct chip was selected, the error window showed below:
the error logs like this:
15:30:23 : UR connection mode is defined with the HWrst reset mode
15:30:23 : 20730746
15:30:23 : Error: J-Link - Connection to target failed
15:30:23 : Error: J-Link - Reading CPUID failed
15:30:23 : Voltage : 3.30V
15:31:20 : Error: Database cannot be found. DatabasePath = D:\ProgramFiles\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/../Data_Base/STM32_Prog_DB_0xFFF.xml
15:31:20 : Error: flash loader cannot be loaded. FlashLoaderPath = D:\ProgramFiles\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0xFFF.stldr
15:31:20 : Error: Database cannot be found. DatabasePath = D:\ProgramFiles\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/../Data_Base/STM32_Prog_DB_0xFFF.xml
I wander if the app support jlink probe, if not, why I can select it?
Solved! Go to Solution.
2024-05-15 01:21 AM
and you're sure it's a genuine J-Link - not a fake/clone?
2024-05-15 05:07 AM
Yes, it was bought on Segger's site.
2024-05-15 05:46 AM
I didn't solve the issue with the J-Link, but I can now program the STM32. I actually found a Nucleo-L433RC and have been able to program the STM32(L052K8) via ST-Link.
2024-05-15 06:39 AM
So there is something wrong with your J-link and/or its setup and/or connections.
Probably best to take that up with Segger:
https://forum.segger.com/index.php/Board/3-J-Link-Flasher-related/