cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer can't see network disk

nico23
Senior III

I've just noticed that STM32CubeProgrammer (2.19.0) can't see network disk on my Windows 10 PC.

I have also set a folder inside of one of the network disk as favourite folder to rapid access on the left sidebar but, when I click it via STM32CubeProgrammer Explorer it says the path is invalid

The network disk is at X://

nico23_0-1741615285777.png

 

4 REPLIES 4
Pavel A.
Super User

Do you run CubeProgrammer as administrator (elevated)?

 

Yes

If it runs under different account (Administrator vs your normal user) it does not see the network shares of the user account. CubeProgrammer normally does not need to run elevated.

 

I'm running on an account that has administrator privilege. The account sees the disks